21  Pairing Bluetooth‎ devices

You can use the camera with the following Bluetooth devices:
  • METERLiNK devices (FLIR meters).
  • Bluetooth-enabled headsets.
If supported by your mobile phone, you can also share the phone’s internet connection with the camera via Bluetooth.
Before you can use a Bluetooth device with the camera, you need to pair the devices. The Bluetooth functionality is managed from the Settings menu. You can also enable/disable Bluetooth on the swipe-down menu. For more information, see section 6.6.5 Swipe-down menu .

Follow this procedure: