22  Fetching data from external FLIR meters

22.1  General

You can fetch data from some external FLIR meters that support Bluetooth and merge this data into the infrared image. When the camera is connected to a FLIR meter via Bluetooth, the measurement value from the meter is displayed in the result table of the camera. The FLIR meter value is also added to the information saved in the image file.
In preview mode and when editing an image in the archive, you can add more than one value from the same FLIR meter. The last added value is displayed below the previous values. The live value is displayed with a dotted outline.
If the screen display for values is full, it is still possible to add more values from the FLIR meter. Added values are then indicated by a box with a number that counts up each time a new value is added.
To find out whether a FLIR meter is supported by the camera, consult the meter documentation.

22.2  Technical support for external meters

Technical support

Website

22.3  Procedure

Follow this procedure:

22.4  Typical moisture measurement and documentation procedure

22.5  More information

For more information, see the user manuals that are shipped with FLIR meters.