13  Working with measurement tools

13.1  General

To measure a temperature, you can use one or more measurement tools, e.g., a spotmeter or a box.
Graphic

13.2  Adding/removing measurement tools

Follow this procedure:

13.3  Editing user presets

A user preset is a measurement tool, or a group of measurement tools, with predefined characteristics.

Follow this procedure:

13.4  Moving and resizing a measurement tool

13.4.1  General

You can move and resize a measurement tool.

13.4.2  Moving a spot

Follow this procedure:

13.4.3  Moving and resizing a box or circle tool

Follow this procedure:

13.5  Changing the measurement parameters

13.5.1  General

For accurate measurements, it is important to set the measurement parameters.

13.5.2  Types of parameters

The camera can use these measurement parameters:
  • External IR window compensation, i.e., the temperature of any protective windows, external lenses (e.g., the close-up lens), etc., that are set up between the camera and the object of interest. If no protective window, protective shield, or external lens is used, this value is irrelevant and should be left inactive.
  • Object distance, i.e., the distance between the camera and the object of interest.
  • Atmospheric temperature, i.e., the temperature of the air between the camera and the object of interest.
  • Relative humidity, i.e., the relative humidity of the air between the camera and the object of interest.
  • Reflected temperature, which is used when compensating for the radiation from the surroundings reflected by the object into the camera. This property of the object is called “reflectivity.”
  • Emissivity, i.e., how much radiation an object emits, compared with the radiation of a theoretical reference object at the same temperature (called a “blackbody”). The opposite of emissivity is reflectivity. The emissivity determines how much of the radiation originates from the object as opposed to being reflected by it.
Emissivity is the most important measurement parameter to set correctly. If the Emissivity is set to a low value, the Reflected temperature also becomes important. The parameters Object distance, Atmospheric temperature, and Relative humidity are relevant for longer distances. The External IR window compensation must be activated if a protective window or external lens is used.

13.5.3  Recommended values

If you are unsure about the values, the following are recommended:
Object distance
1.0 m (3.3 ft.)
Atmospheric temperature
20°C (69°F)
Relative humidity
50%
Reflected temperature
20°C (69°F)
Emissivity
0.95

13.5.4  Procedure

You can set the measurement parameters globally. You can also change the Emissivity, Reflected temperature, and Object distance parameters locally for a measurement tool.
Local parameters are normally only effective for a fixed setup, where each measurement tool is set for a specific object of interest. For a general handheld application, the global parameters are usually sufficient.

13.5.4.1  Setting global parameters

Follow this procedure:

13.5.4.2  Changing local parameters

You can change the local parameters for a measurement tool.
A P next to the measurement tool on the screen indicates that local parameters have been activated for the tool.

Follow this procedure:

13.6  Displaying values in the result table

For the box and circle tools, you can set the camera to display the maximum, minimum, average, and area values in the result table.

Follow this procedure:

13.7  Creating and setting up a difference calculation

A difference calculation gives the difference between the values of two known measurement results.

Follow this procedure:

13.8  Setting a measurement alarm

13.8.1  General

You can make the camera trigger an alarm when certain measurement conditions are met.

13.8.2  Types of alarm

You can choose between the following alarm types:
  • Above: Triggers an alarm when the temperature is above the preset alarm temperature.
  • Below: Triggers an alarm when the temperature is below the preset alarm temperature.

13.8.3  Alarm signals

When an alarm is set, the symbol icon is displayed in the result table.
When an alarm is triggered, the value in the result table is displayed in red (above alarm) or blue (below alarm) and the symbol icon (above alarm) or icon (below alarm) is blinking.
You can also set an audible alarm (there will be a “beep” when the alarm is triggered).

13.8.4  Procedure

There are different procedures for setting up an alarm for a spot, for a box or circle, and for a difference calculation.

13.8.4.1  Setting up an alarm for a spot

Follow this procedure:

13.8.4.2  Setting up an alarm for a box or circle

Follow this procedure:

13.8.4.3  Setting up an alarm for a difference calculation

To set up an alarm for a difference calculation, do the following: