6  Camera overview

6.1  View from the rear

Graphic

6.2  View from the front

Graphic

6.3  View from the bottom

Graphic

6.4  Laser distance meter and laser pointer

The laser distance meter consists of a laser transmitter and a laser receiver. The laser transmitter also works as a laser pointer.

6.4.1  Laser transmitter and receiver

Graphic

6.4.2  Difference in position

This figure shows the difference in position between the laser transmitter and the optical center of the infrared lens. The laser transmitter and the optical axis are parallel.
Graphic

6.4.3  Laser warning label

A laser warning label with the following information is attached to the camera:
Graphic

6.4.4  Laser rules and regulations

Wavelength: 650 nm. Maximum output power: 1 mW.
This product complies with 21 CFR 1040.10 and 1040.11 except for deviations pursuant to Laser Notice No. 50, dated June 24, 2007.

6.5  Screen elements

6.5.1  General

Graphic

6.5.2  Menu system

To display the menu system, push the navigation pad or tap the menu system button Graphic .
Graphic

6.5.3  Soft buttons

Graphic

6.5.4  Status icons and indicators

icon
Battery level
  • Green: above 75%
  • Yellow: up to 75%
  • Red: up to 25%
  • No color: below 15%
icon
The remaining storage capacity of the memory card is below 100 MB.
icon
The GPS is enabled.
If the icon is grey, the camera cannot find a GPS signal.
icon
External infrared window compensation is enabled.
icon
icon
The camera is paired with a FLIR Ignite account.
The camera is paired, but does not have contact with FLIR Ignite (no internet connection).
icon
A Bluetooth headset is connected.
icon
The laser is on.

6.5.5  Swipe-down menu

To open the swipe-down menu, place your finger at the top of the screen and swipe down.
Graphic

6.5.6  Image overlay information

The image information consists of items such as the date, emissivity, and atmospheric temperature. All image information is saved in the image file and can be viewed in the image archive. You can also choose to display selected items as image overlay information. All image overlay information displayed on the live image will also be displayed on saved images. For more information, see sections section 23.5 Device settings and 11.8 Hiding all overlay .
Graphic

6.6  Navigating the menu system

    You can navigate the menu system in two ways:
  • Using your finger or a stylus pen specially designed for capacitive touch usage.
  • Using the navigation pad and the back button icon .
Graphic
Graphic

6.6.1  Navigating using the navigation pad

You navigate the menu system by using the navigation pad and the back button:
  • To display the menu system, push the center of the navigation pad.
  • To navigate in menus, submenus, and dialog boxes, and to change values in dialog boxes, push the navigation pad up/down or left/right.
  • To confirm changes and settings in menus and dialog boxes, push the center of the navigation pad.
  • To leave dialog boxes and to go back in the menu system, push the back button icon .