11  Achieving a good image

11.1  General

A good image depends on several different functions and settings, although some functions and settings affect the image more than others.
These are the functions and settings that you need to experiment with:
  • Adjusting the infrared camera focus.
  • Adjusting the infrared image (automatically or manually).
  • Selecting a suitable temperature range.
  • Selecting a suitable color palette.
  • Changing the measurement parameters.
  • Performing a non-uniformity correction (NUC).
The following sections explain how to work with these functions and settings.
In some situations, you may also want to hide the overlay graphics for a better view.

11.2  Adjusting the infrared camera focus

It is very important to adjust the focus correctly. Incorrect focus adjustment affects how the image modes work. It also affects the temperature measurement.

11.2.1  Manual focus

You can adjust the focus manually by rotating the focus ring. For more information, see section 7.4.1 Manual focus .

11.2.2  Autofocus

You can autofocus the infrared camera by pushing the Autofocus button. For more information, see section 7.4.2 Autofocus .

11.2.3  Continuous autofocus

The infrared camera can be set up to perform continuous autofocusing. For more information, see section 7.4.3 Continuous autofocus .

11.3  Adjusting the infrared image

11.3.1  General

An infrared image can be adjusted automatically or manually.
In automatic mode, the camera continuously adjusts the level and span for the best image presentation, using one of the following color distribution methods:
  • Histogram: The colors are distributed based on the thermal content of the image.
  • Linear: The colors are distributed evenly from the lowest to the highest temperature.
The color distribution method for the automatic mode is configured by a setting. Select icon (Settings) > Device settings > User interface options > Auto adjustment method.
By using the Auto adjustment region feature it is possible to select an area of the image, and then have the colorization of the image adjusted based on the temperatures within that selected area. For more information, see section 11.3.2 Auto adjustment region .
In manual mode, you can adjust the temperature scale to values close to the temperature of a specific object in the image. This will make it possible to detect anomalies and smaller temperature differences in the part of the image of interest. In manual mode, the colors are distributed evenly from the lowest to the highest temperature (linear color distribution).
In manual mode, you can adjust the image by touching the screen or by using the navigation pad. For more information, see sections 11.3.3 Manual adjustment by touching the screen and 11.3.4 Manual adjustment by using the navigation pad .
  • In live mode, touch the soft button icon to switch between automatic and manual image adjustment modes.
  • In preview/edit mode, manual image adjustment mode is active.

11.3.1.1  Example 1

Here are two infrared images of a building. In the left image, which is auto-adjusted, the large temperature span between the clear sky and the heated building makes a correct analysis difficult. You can analyze the building in more detail if you change the temperature scale to values close to the temperature of the building.
Graphic
Automatic
Graphic
Manual

11.3.1.2  Example 2

Here are two infrared images of an isolator in a power line. To make it easier to analyze the temperature variations in the isolator, the temperature scale in the right image has been changed to values close to the temperature of the isolator.
Graphic
Automatic
Graphic
Manual

11.3.2  Auto adjustment region

When you auto-adjust a thermal image, you adjust it for the best image brightness and contrast. This means that the color information is distributed over the existing temperatures of the image.
In some situations, the image may contain very hot or very cold areas outside your area of interest. In such cases you might want to exclude those areas and use the color information only for the temperatures in your area of interest. You can do so by selecting a smaller auto adjustment region.
Select the auto adjustment region under icon (Settings) > Device settings > User interface options > Auto adjustment region.

11.3.3  Manual adjustment by touching the screen

11.3.3.1  General

The touch functionality for manual image adjustments is enabled/disabled by a setting. Select icon (Settings) > Device settings > User interface options > Manual adjustment using touch > On/Off.
When manual image adjustment mode is active, an adjustment wheel is displayed to the right of the temperature scale. (Applicable when the manual adjustment by touch functionality is enabled.)
Graphic

Figure 11.1  Manual adjustment mode active

11.3.3.2  Procedure

11.3.3.3  Auto-adjusting the image in manual mode

In manual image adjustment mode, you can auto-adjust the image by touching the screen. The image will be auto-adjusted based on the thermal content of the area around the touched point. The top and bottom levels in the temperature scale will be set to the maximum and minimum temperatures in that area. By using the color information only for the relevant temperatures, you will get more details in your area of interest.
Graphic

11.3.3.4  Locking the touch screen

When you have adjusted the image to levels that allow you to study your area of interest, you can lock the touch screen to prevent further unintentional adjustments.
To lock the screen, touch the icon icon to the left of the temperature scale.
To unlock the screen, touch the icon icon to the left of the temperature scale.

11.3.4  Manual adjustment by using the navigation pad

11.3.4.1  Manual adjustment modes

There are two different settings for the manual adjustment mode (applicable for the navigation pad only):
  • Level, Span: With this setting, you can manually adjust the level and span by using the navigation pad.
  • Level, Max, Min: With this setting, you can manually adjust the level by using the navigation pad. You can also change the upper and lower temperatures individually.
Select the type of manual image adjustment mode under icon (Settings) > Device settings > User interface options > Manual adjustment mode.

11.3.5  Manual adjustment in Level, Span mode

Follow this procedure:

11.3.6  Manual adjustment in Level, Max, Min mode

Follow this procedure:

11.4  Changing the camera temperature range

The camera is calibrated for different temperature ranges. Available temperature range options are dependent on the camera model.
For accurate temperature measurements, you must change the Camera temperature range setting to suit the expected temperature of the object you are inspecting.

Follow this procedure:

11.5  Changing the color palettes

You can change the color palette that the camera uses to display different temperatures. A different palette can make it easier to analyze an image.
This table explains the different types of color palettes.
Graphic
Iron
Graphic
Arctic
Graphic
Rainbow
Graphic
Rainbow high contrast
Graphic
White hot
Graphic
Black hot
Graphic
Lava
 

Follow this procedure:

11.6  Changing the measurement parameters

For accurate measurements, it is important to set the measurement parameters:
  • Emissivity.
  • Reflected temperature.
  • Object distance.
  • Atmospheric temperature.
  • Relative humidity.
  • External IR window compensation.
Emissivity is the most important measurement parameter to set correctly. If the Emissivity is set to a low value, the Reflected temperature also becomes important. The parameters Object distance, Atmospheric temperature, and Relative humidity are relevant for longer distances. The External IR window compensation must be activated if a protective window or external lens is used.
You can set the measurement parameters globally. You can also change the Emissivity, Reflected temperature, and Object distance parameters locally for a measurement tool.
For more information, see section 13.5 Changing the measurement parameters .

11.7  Performing a non-uniformity correction (NUC)

11.7.1  General

When the thermal camera displays Calibrating... it is performing what in thermography is called a ”non-uniformity correction” (NUC). An NUC is an image correction carried out by the camera software to compensate for different sensitivities of detector elements and other optical and geometrical disturbances 6 . For more information, see section 28 About calibration .
An NUC is performed automatically, for example at start-up, when changing a measurement range, or when the environment temperature changes.
You can also perform an NUC manually. This is useful when you have to perform a critical measurement with as little image disturbance as possible. You may, for example, want to perform a manual calibration just before you start recording a video sequence.

11.7.2  Performing an NUC manually

To perform a manual NUC, push and hold down the image archive button icon for more than 2 seconds.

11.8  Hiding all overlay

The camera overlay consists of overlay graphics and image overlay information. The overlay graphics include items such as measurement tool symbols, result tables, and status icons. The image overlay information, which you activate on the Settings menu, provides additional information such as the date, emissivity, and atmospheric temperature. For more information, see section 6.5.6 Image overlay information .
You can hide all camera overlay by touching the soft button icon .
Graphic
Image with camera overlay and image overlay information.
Graphic
Image with all overlay hidden.