Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Measurement) and push the navigation pad. This displays a submenu.
Use the navigation pad to select one of the following:
Push the navigation pad to confirm and exit the menu mode.
Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Measurement) and push the navigation pad. This displays a submenu.
Use the navigation pad to select
(User preset 1) or
(User preset 2).
Push and hold the center of the navigation pad. This displays the Edit user preset menu.
Select
(Add measurement) and push the navigation pad. This displays a submenu.
Use the navigation pad to select one of the following:
Push the navigation pad. This displays the measurement tool on the screen.
Push the navigation pad. This displays a context menu, where you can select one or more of the following actions (depending on the type of tool):
When all measurement tools have been added, select
(Save as user preset).
Push the navigation pad to confirm and exit the menu mode.
Follow this procedure:
To select the spot, touch the tool on the screen. The tool is now displayed with a frame.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
To move the spot, do the following:
To center the spot, select
Center spot and push the navigation pad.
When completed, push the navigation pad and select
(Done).
Push the navigation pad to confirm and exit the menu mode.
Follow this procedure:
To select the measurement tool, touch the tool on the screen. The tool is now displayed with one or more handles.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
Select
(Move/resize) and push the navigation pad. This displays a submenu.
Use the navigation pad to select one of the following:
Push the navigation pad up/down and left/right to resize or move the tool.
When completed, push the navigation pad and select
(Done).
Push the navigation pad to confirm and exit the menu mode.
|
Object distance
|
1.0 m (3.3 ft.)
|
|
Atmospheric temperature
|
20°C (69°F)
|
|
Relative humidity
|
50%
|
|
Reflected temperature
|
20°C (69°F)
|
|
Emissivity
|
0.95
|
Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Measurement parameters) and push the navigation pad. This displays a submenu.
Use the navigation pad to select one or more of the global measurement parameters:
Push the navigation pad to display a dialog box.
Use the navigation pad to change the parameter.
Push the navigation pad to confirm and exit the menu mode.
Follow this procedure:
To select the measurement tool, touch the tool on the screen. The tool is now displayed with one or more handles.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
Select
(Use local parameters) and push the navigation pad.
Push the navigation pad to activate the use of local parameters. This displays a submenu.
Use the navigation pad to select one or more of the local measurement parameters.
Push the navigation pad to display a dialog box.
Use the navigation pad to change the parameter.
Push the navigation pad. This closes the dialog box.
When completed, push the navigation pad and select
(Done).
Push the navigation pad to confirm and exit the menu mode.
Follow this procedure:
To select the measurement tool, touch the tool on the screen. The tool is now displayed with one or more handles.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
Use the navigation pad to select
(Max/Min/Avg).
Push the navigation pad. This displays a submenu.
Use the navigation pad to select one or more of the following:
Push the navigation pad to toggle the function between inactive and active.
When completed, push the navigation pad down to close the submenu.
Select
(Done) and push the navigation pad.
Follow this procedure:
To set up a difference calculation, do the following:
Push the navigation pad. This displays a dialog box where you can select the measurement tools that you want to use in the difference calculation. You can also select a fixed-temperature reference.
Push the navigation pad. The result of the difference calculation is now displayed on the screen.
Follow this procedure:
To select the spot, touch the tool on the screen. The tool is now displayed with a frame.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
Select
(Set alarm on spot) and push the navigation pad. This displays a dialog box.
In the dialog box, you can define the settings for the alarm.
Push the navigation pad. This closes the dialog box.
Follow this procedure:
To select the measurement tool, touch the tool on the screen. The tool is now displayed with one or more handles.
Push the navigation pad—or touch and hold the tool. This displays a context menu.
Select
(Set alarm) and push the navigation pad. This displays a dialog box.
In the dialog box, you can define the settings for the alarm.
Push the navigation pad. This closes the dialog box.
To set up an alarm for a difference calculation, do the following:
If you are editing an image in the archive, select
(Measurement).
Select
(Select) and push the navigation pad. This displays a dialog box.
Select Delta and push the navigation pad. This displays a context menu.
Select
(Set alarm on delta) and push the navigation pad. This displays a dialog box.
In the dialog box, you can define the settings for the alarm.
Push the navigation pad. This closes the dialog box.