To enable High Sensitivity Mode (HSM), do the following:
Push the navigation pad to display the menu system.
Select
(Image mode) and push the navigation pad. This displays a submenu.
Select
(HSM) and push the navigation pad.
To adjust the temperature scale, do the following:
Touch the soft button
to enter manual image adjustment mode.
Do one or more of the following:
To prevent further unintentional adjustments, you can lock the touch screen.
To change the color palette, do the following:
Push the navigation pad to display the menu system.
Select
(Color) and push the navigation pad. This displays a submenu.
Use the navigation pad to select a different palette.
Push the navigation pad to confirm and exit the menu mode.