If you plan to run the screening station 24/7 without any operator interaction, you may want to enable some automatic functions.
6.5.1 Automatic reset of moving average
If there has been a long time since the last screening, the moving average may not be at the correct level and there is a
risk for false negatives. One way of limiting this risk is to reset the moving average, manually or automatically. The system
will then start to build up a new moving average. For more information, see section
10.4.3.1 Reset of moving average
.
After an automatic reset of the moving average, the system will evaluate also the first screened person (which is not the case after a manual
reset). Since there is no average to compare with after the reset, a fixed temperature value will be used for the evaluation
of the first person.
The default fixed temperature value can be used as a starting point. However, the appropriate value depends on factors such
as environmental conditions and time of day. It is recommended to establish a fixed temperature value adapted to your local
conditions.
6.5.1.1 Establish fixed temperature value
The fixed temperature value can be established by checking the measured temperatures in FLIR Screen-EST at the same time for three days in a row and then use the highest of these temperatures.
Note
You may need to adjust the fixed temperature value as conditions change, for example due to seasonal variations.
To establish the fixed temperature value, do the following:
-
Make a decision on the likely time for the first person to enter the screening station after a reset of the moving average.
-
At the same time (as decided above) for three days in a row, check the operator window and make a note of the measured temperatures.
-
Use the highest of the recorded temperatures as your fixed temperature value.
6.5.1.2 Enable automatic reset
To enable automatic reset of the moving average, do the following:
-
Open the Settings page, see section
6.4.1 Open the Settings page
.
-
On the Face detection tab, select the Reset moving average after specified time check box.
-
In the Reset after fields, enter the time (hours:minutes).
-
In the Temperature after reset field, enter your fixed temperature value (see section
6.5.1.1 Establish fixed temperature value
).
6.5.2 Automatic restart of screening
Windows devices are sometimes forced to restart, for example after a Windows update, which also closes all applications. The
device may also shut down completely if the battery level is very low. By a setting, you can ensure that FLIR Screen-EST starts up automatically when the device restarts.
There is also a setting that will make FLIR Screen-EST restart automatically after an unexpected crash or if the application is not responding.
FLIR Screen-EST stores all settings and states, including the moving average, during an on-going screening session. When an automatic function
starts FLIR Screen-EST after an unexpected system restart or application failure, the stored values will be used and the screening can continue
without any operator interaction.
Note
When you manually close FLIR Screen-EST, the moving average is reset. This means that the system will start to build up a new baseline for the moving average when
FLIR Screen-EST starts up the next time.
To enable automatic restart of the screening, do the following:
-
Open the Settings page, see section
6.4.1 Open the Settings page
.
-
On the General tab, do the following:
-
Select the Start application on system start-up check box to enable automatic start of FLIR Screen-EST.
-
Select the Enable application monitoring check box to enable automatic restart after an application failure.
-
In the operator window, make sure the Auto-reconnect check box is selected. This will make the camera connect automatically, allowing the screening to start again.