To adjust the temperature scale, do the following:
Touch the soft button
to enter manual image adjustment mode.
Do one or more of the following:
To prevent further unintentional adjustments, you can lock the touch screen.
Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Settings) and push the navigation pad. This displays the Settings menu.
Select Camera temperature range and push the navigation pad. This displays a dialog box.
Select the appropriate temperature range and push the navigation pad.
To change the color palette, do the following:
Push the navigation pad to display the menu system.
Select
(Color) and push the navigation pad. This displays a submenu.
Use the navigation pad to select a different palette.
Push the navigation pad to confirm and exit the menu mode.
To perform a manual NUC, push and hold down the image archive button
for more than 2 seconds.