To preview an image, do the following:
To preview an image, push the Save button. This displays the preview.
Manual image adjustment mode is now active. For image adjustment instructions, see section 11.3 Adjusting the infrared image .
To edit the image, push the navigation pad. This displays a context menu. For editing instructions, see section 8.5 Editing a saved image .
Do one of the following:
To open a saved image, do the following:
Push the image archive button
. This displays the Gallery with one or more folders.
Select a folder and push the navigation pad.
Select the image you want to view and push the navigation pad.
Do one or more of the following:
To edit a saved image, do the following:
Push the image archive button
. This displays the Gallery.
Select a folder and push the navigation pad.
Select the image you want to edit and push the navigation pad.
Push the navigation pad to display the top toolbar.
On the top toolbar, select the
icon and push the navigation pad.
On the right toolbar, select the
icon and push the navigation pad. This opens the image in edit mode.
Manual image adjustment mode is now active. For image adjustment instructions, see section 11.3 Adjusting the infrared image .
Push the navigation pad. This displays a context menu.
To store the edited image online, make a manual upload of the image. See section 9.6 Manual upload .
To display the image information, do the following:
Push the image archive button
. This displays the Gallery.
Select a folder and push the navigation pad.
Select an image and push the navigation pad.
Push the navigation pad to display the top toolbar.
On the top toolbar, select the
icon and push the navigation pad.
On the right toolbar, select the
icon and push the navigation pad. This displays the image information.
Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Settings) and push the navigation pad. This displays the Settings menu.
Use the navigation pad to select Device settings > Reset options > Reset image counter....
Push the navigation pad. This displays a dialog box.
To reset the counter, select Reset and push the navigation pad.